| TraceParts help |
| System requirements | Installation/Uninstallation | Quick start | Registration | |
| Interface | Configuration | Use | Advanced use | |
| FAQ | Troubleshooting | Glossary | ||
Type of installation that install only the "APPLICATION" parts of TraceParts. This type of installation can be performed only if a COMPLETE installation has already been performed on another computer and its catalogs shared. Type of installation that install both application and catalogs of TraceParts. Hardware protection device plugged on the USB or parallel ports TraceParts can use three types of dongle: Each of these dongles requires a specific driver that are automatically installed with TraceParts. Mode of operation of TraceParts in which the library works with no functionnality limitation but with duration limitation. TraceParts will stop working 10 days after its installation. This is the default operation mode of TraceParts. Type of license that allow the use of TraceParts at the same time on "n" computers when TraceParts is installed on "x" computers (x>n). We talked of license "n" workstation, or floating license "n" tokens. Depending of the context: In this document, "License" will always referes to the protection system of TraceParts. Type of installation that prepares a deployment folder containing an unattended installation of TraceParts. The deployment folder contains ONLY the required files to meet the user request. Software components made by Microsoft and required for TraceParts. Software component from Microsoft that allow TraceParts to use databases. MDAC can be downloaded on the page "MDAC Downloads" of Microsoft website. Software component from Microsoft that allow TraceParts to use ACCESS databases. MSJET can be downloaded on the page "MDAC Downloads" of Microsoft website. Software component from Microsoft that allow TraceParts to run scripts. A network installation is when TraceParts is installed on several computers from a network that share the same catalogs. NLM = Network Licence Manager This is the software use by TraceParts to use floating license. NTFS (New Technology File System) is a file system created by Microsoft for Windows NT 4. The current version is version 3.1, it is embedded in Windows XP, 2003 and Vista. This is the only file system that can handle the large amount of files used by TraceParts. A "Product" is a variation of TraceParts for a specific manufacturer. For example, there is a product for manufacturer "RABOURDIN", another for "LEGRIS", another for "BOUTET", etc. Each product contains only the catalog of the manufacturer related to it. Note: Standard TraceParts DVD is also called "Standard product". Refere to "Licence". Mode of operation of TraceParts in which the library works with no limitation. This is the operation mode of TraceParts once the license has been installed. Licence that allow the use of TraceParts on all the computers of a school. Type of license that allow the use of TraceParts on only one computer. UNC = Universal Naming Convention Path compliant with the Universal naming convention. Such a path is like: \\server name\share A "version" of TraceParts is a number that correspond to the state of TraceParts(in terms of application and content) at the time of its delivery. Each version has a unique number. Notes: [ Back to the top ] |
||||