TraceParts installation guide


Read me first Installations types Complete Application
Catalogs only Massive deployment Network installation Registration
Use FAQ Glossary Uninstallation
 
Before you start


Thanks for choosing TraceParts.

Before start, please note:
  • All of our DVDs will install TraceParts in trial mode. TraceParts will run in registered mode once the protection system is installed.
  • The user that will install TraceParts MUST have administrator rights,
  • The CAD programs to be used with TraceParts have to be installed locally on each of the PC.
  • The CAD programs to be used with TraceParts MUST have been launched at least one time before installing TraceParts.
Already TraceParts users:

If TraceParts has already been installed on the computer (any version)

If the installation has been done more than 10 days ago, the new installation will be done, but will give an error at the end, telling the trial period has expired.

If so..

..if you are a customer:
Then just end the installation by clicking the "Cancel" button (of the protection dialog box) and install the protection system you have purchased(code, dongle, school license or floating license).

..if you are not a customer yet:
Except buying TraceParts, you can extend the trial period once, by filling the form here:
http://www.traceparts.com/support/helpdesk.asp


IMPORTANT
  • If a version prior to TraceParts v2.5.0. is currently installed on the computer where you are about to install the new version of TraceParts:
    • The previous TraceParts version must be uninstalled

  • If the installed version or product is the same as the one you are about to install : STOP!

    Indeed:
    1. The version/product you are about to install is the same as the one already installed, even if you have bought it, it is useless to loose time reinstalling it again.
    2. This is the protection system that makes a trial version a registered version, so the already installed version will work the same as the one you wanted to install,
    3. If you did not install all the catalogs, or if you want to uninstall some catalogs, please refer to the TraceParts user manual, "Advanced use" section, chapter "Add or Remove Parts Catalogs"

  • Antivirus: It is recommended to disable antivirus the time of installation

System requirements

Operating systems
Microsoft Windows

Compatibilities
Type Version Compatible
Windows VISTA - 32 bits Business/Ultimate Yes
Windows VISTA - 32 bits Home No
Windows VISTA - 64 bits All versions No
Windows 2003 - 32/64 bits All versions Yes
Windows XP Pro - 32/64 bits All versions Yes
Windows XP Home 32 bits All versions No
Windows 2000 Pro All versions Yes
Windows 2000 Server All versions Yes
Windows 2000 Advanced Server All versions Yes
Any other Windows -- No


Required Microsoft components
Whatever the version of Windows used, the following components must be present on the PC where TraceParts is installed:
Component Minimum required version Note
Internet Explorer IE 5.5. IE6 SP1 recommended.
Microsoft Data Access Component (MDAC) MDAC 2.6 Installed automatically by TraceParts if necessary
Microsoft JET Engine MS JET 4 SP3 Installed automatically by TraceParts if necessary
Microsoft Scripting Runtime 5.5 Installed automatically by TraceParts if necessary
Microsoft XML Parser 3 SP1 Installed automatically by TraceParts if necessary


Other Operating Systems

TraceParts is available only for Windows and cannot be used on other operating systems, in particular UNIX or LINUX. 


Internet connection
Some parts requires an Internet connection to be used.


Compatible CAD Software
Notes:
    1. TraceParts and its associated CAD program MUST be installed on the same PC..
    2. Unless specified, all CAD software mentionned below are 32bits CAD programs.

Alibre
Software Versions Compatible
Alibre Design Prior to v 8.2 No
After or equal to v 8.2 Yes

ASCON
Software Versions Compatible
Kompas-3D Prior to v9 No
After or equal to v9 Yes

Autodesk
Software Versions Compatible
AutoCAD LT All versions No
AutoCAD Versions prior to 2004 No
Versions after or equal to 2004 Yes
AutoCAD Mechanical All versions equal to or after 2004 (including DX) Yes
AutoCAD Mechanical Desktop Versions prior to 2004 No
Versions after or equal to 2004 Yes
Inventor Versions prior to v5.3 No
Versions after or equal to v5.3 Yes
Inventor - 64 bits Versions prior to 2009 No
Versions after or equal to 2009 Yes
Inventor professional Versions prior to v5.3 No
Versions after or equal to v5.3 Yes
Inventor Professional- 64 bits Versions prior to 2009 No
Versions after or equal to 2009 Yes

Dassault Systèmes
Software Versions Compatible
CATIA V4 All versions No
CATIA V5 Prior to CATIA V5R13GA No
After or equal to CATIA V5R13GA Yes
CATIA V5 - 64 bits Prior to CATIA V5R16GA No
After or equal to CATIA V5R16GA Yes

PTC
Software Versions Compatible
Pro/ENGINEER 2001 Before build 240 No
After or equal to build 240 Yes
Pro/ENGINEER Wildfire 1.0 All versions Yes
Pro/ENGINEER Wildfire 2.0 All versions Yes
Pro/ENGINEER Wildfire 3.0 All versions Yes
Pro/ENGINEER Wildfire 4.0 All versions Yes
Pro/ENGINEER Wildfire 4.0 - 64bits All versions Yes

SolidWorks
Software Versions Compatible
SolidWorks (including office and professional) Prior to 2001+ SP6.0 No
After or equal to 2001+ SP6.0 Yes

Solid Edge
Software Versions Compatible
Solid Edge Prior to v10SP8 No
v10SP8 to v19 Yes
Solid Edge - 64 bits All versions No

think3
Software Versions Compatible
thinkdesign Prior to v8.4 No
After or equal to v8.4 Yes

Missler Software
Software Versions Compatible
TopSolid Prior to 2003 (=6.5) No
After or equal to 2003(=6.5) Yes



File formats supported
In addition to the formats corresponding to the above software, TraceParts can generate files in the following formats:

3DXML
File extension Versions Compatible
.3dxml Prior to v4 No
After or equal to v4 Yes

ACIS
File extension Versions Compatible
.sat Prior to 6.3 No
After or equal to 6.3 Yes

CATIA V4
File extension Versions Compatible
.model All versions Yes

Granite One
File extension Versions Compatible
.g Prior to v3 No
After or equal to v3 Yes

IGES
File extension Versions Compatible
.igs All versions Yes

Images
File extension Versions Compatible
.BMP
.PNG
.GIF
.JPEG
.TIFF
.RLE
.PCX
.PGA
Any version Yes

Parasolid
File extension Versions Compatible
.x_t Prior to 11.1 No
After or equal to 11.1 Yes

SketchUp
File extension Versions Compatible
.skp Version 5 Yes

STEP
File extension Versions Compatible
.stp AP203 & AP214 Yes

VRML
File extension Versions Compatible
.wrz VRML97 and higher Yes



Hardware
Specifications
Processor : 32 or 64-bit with at least Intel Pentium III or AMD Athlon processor
RAM : Minimum 256 MB of RAM, 512 MB for CATIA V5
Video : 3D graphic card, display in 1024x768, supporting OpenGL

Note: The computer must have a DVD driver.

Disk requirements
Warning
  • Because of the large number of files required by TraceParts, it is strongly recommended that the partition on which the TraceParts catalogs are installed be formatted in NTFS.
  • ATI users: it is advisable to disable hardware acceleration from TraceParts configuration.
Requirements
  • 100 MB free on the disk where Windows is installed (if all possible CAD drivers are selected);
  • 10 MB free for installation of the application;
  • 2 GB free for installation of the catalogs.
  • 500 Mb free in the temp directory of the current user


  • Optional Software
    Adobe Acrobat Reader
    This program may be needed to open certain documents linked to the parts. It can be downloaded here: http://www.adobe.com/


    [ Back to the top ]