webleads-tracker

Home > TraceParts for Developers > Number of part numbers

Introduction

Find the number of unique part numbers for one catalog, one category or one product.

 

API Key

This web service requires an API Key. Please refer to this chapter to request your API Key.

 

Description

This API returns the number of unique part numbers depending on the level of data. The number of part numbers is only for the ones which can be predefined. If a part number depends on a manual input, it can not be counted. The number includes the sum of all the sub products under the selected level (catalog or category).

 

Building a URL

The CountPartNumbers API request takes the following form:

http://ws.tracepartsonline.net/tpowebservices/CountPartNumbers?parameters

 

Parameters

Certain parameters are required while others are optional. As is standard in URLs, all parameters are separated using the ampersand (&) character. The list of parameters and their possible values are enumerated below.

 

Required parameters

Parameter Name

Data type

Default value

Description

ApiKey

string

none

Code calling an API to track and control how the API is used

Format

string

none

Answer file type (xml, json or csv)

ClassificationID

string

none

CatalogID given by the CatalogsList API

 

Optional parameters

Parameter Name

Data type

Default value

Description

Path

string

root of the catalog

Category path which contents a list of product(s) given by the CategoriesList API

PartID

string

none

Product ID given by the ProductsList

UserEmail

string

none

User email / User ID

ActiveJsonLight

boolean

0

Enables the light version when json is the answer file type

Example of CountPartNumbers API

The request below returns the number of part numbers for the ASCO Numatics catalog, for the “Pneumatics” category, as an xml file.

http://ws.tracepartsonline.net/tpowebservices/CountPartNumbers?ClassificationId=ASCO_JOUCOMATIC&Path=/F_ASJC/F_ASJC.ASJC1/&Format=xml&ApiKey={ApiKey}

By changing the Format and adding the ActiveJsonLight, CountPartNumbers returns the number, as a light Json file.

http://ws.tracepartsonline.net/tpowebservices/CountPartNumbers?ClassificationId=ASCO_JOUCOMATIC&Path=/F_ASJC/F_ASJC.ASJC1/&Format=json&ActiveJsonLight=1&ApiKey={ApiKey}

CountPartNumbers responses

CountPartNumbers responses are returned in the format indicated by the Format parameter within the URL request’s path.

 

JSON Output

A sample HTTP request is shown below, displaying the number of part numbers.

{
"count":"140584",
}

 

XML Output

Same example as above.

<WsCountPartNumbers>
<Count>140584</Count>
</WsCountPartNumbers>

CountPartNumbers response elements

CountPartNumbers responses contain one element:

  • “count”: it is the number of unique part numbers in all products of the current catalog/category and the sub categories

Developer support

Please contact us for any problems, questions or comments related to this web service.

Last updated September 26, 2017